Semiconductor & Devices


Mitsubishi Electric provides semiconductors/devices including power modules and high power devices that handle the highly efficient control of power, optical devices that deliver the performance required in fibre-optic communication devices, high frequency devices that cover everything from radios and mobile phones to satellite communications, and the line of TFT-LCD modules that improve interfaces for information.

Power Modules

Power Modules

Mitsubishi Electric power modules are manufactured with state-of-the-art technologies that ensure the highest levels of performance and reliability while offering impressive energy savings for the products and systems they're used in.

High-Power Devices

High-Power Devices

High-power devices contribute to increased efficiency and energy savings by supporting the high-voltage, high-current and usage environment of rollers in steel works, electric power systems and the subway.

Driver IC, Sensors

Driver IC, Sensors

Mitsubishi Electric's line-up of power semiconductors include transistor arrays, HVICs (High-Voltage IC) and sensors. Using the output from a 3-volt microcomputer, our transistor arrays make possible bufferless direct drive, helping contribute to lighter weight and more compact design in a variety of equipment.

Optical Devices

Optical Devices

Mitsubishi Electric is at the forefront of industry in the development and production of laser diodes and modules, including the latest optical fibre communications for broadband and telecommunications networks, and laser diodes for display and industrial applications.

TFT-LCD Modules

TFT-LCD Modules

Mitsubishi Electric's thin-film-transistor liquid-crystal display (TFT-LCD) modules are built for a wide variety of industrial uses, such as for measuring instruments, automatic teller machines (ATM), point-of-sale terminals (POS), factory automation equipment (FA) and more.

igh-Frequency Devices

High-Frequency Devices

Mitsubishi Electric has long supported the advancement of wireless communication networks through the development of its high frequency devices. Products manufactured utilising the latest electronics and other technologies combined with newly developed high-performance materials have kept us in a market leading position.

Related
Case Studies

Here are case studies that highlight India’s dream to be No.1. Rest assured, we are striving hard to make them turn real.

Browse All

Get in Touch

Contact Us