IT COOLING SYSTEMS
1 Nov. 2022
Mitsubishi Electric Hydronics & IT Cooling Systems, through its brand RC has supplied the HPAC units for the WIIT Data Center in Milan. WIIT is an Italian company focused on Private and Hybrid Cloud continuative services, and is one of the main players in Europe and Worldwide, specialized in application management and critical applications such as disaster recovery and business continuity. WIIT owns three data centers in Italy.

The Milan Data Center has a surface of 550 sq. metres. It is the company’s primary Data Center where the most complex ERP (Enterprise Resource Planning) infrastructure is located and managed. The structure achieved Tier IV certification from the Uptime Institute.

RC’s solution has supplied a high energy savings, fully redundant cooling system for this TIER IV certified Data Center. Going in detail 10 NEXT EVO INV DX U and 18 remote condensers TEAM MATE STD have been installed. NEXT EVO INV DX U direct expansion precision air conditioners equipped with BLDC inverter scroll compressor matched with TEAM MATE remote air cooled condensers represent a perfect example of reliability and efficiency. The use of direct free cooling increases the efficiency of the system.