Mitsubishi Electric’s MS-GK series AC – The best eco-friendly AC that there is
For many homes, the biggest sign of an air conditioner getting old is the rising electricity bills. However, what many do not notice is how ageing air conditioners are impacting the quality of life and the world in general. With environmental issues that are expected to pose long-term effects, the need for smarter air conditioners has become more pronounced.
Mitsubishi Electric India (MEI), as a progressive and responsible brand, is playing its part in building a better tomorrow by creating solutions that are not only smart and practical but also on the side of Mother Nature.
The MS-GK series of air conditioners by MEI is one such appliance that is at the core of this philosophy.
What makes Mitsubishi Electric’s MS-GK series ACs eco-friendly?
Mitsubishi Electric’s MS-GK series of air conditioners comprise of many features and functions that make it a smart and environment-friendly appliance. Prime among these features are: -
- Use of R410A refrigerant – Unlike standard ACs that use HCFCs or hydrochlorofluorocarbons, compounds that are condemned for their ozone-depleting characteristics, the MS-GK series of air conditioners by MEI utilize R410A for cooling. This is a chlorine-free, eco-friendly, non-inflammable and energy efficient alternative that is known to have no ozone depleting potential.
- Econo-cool for smart savings – A single-touch operation feature, Econo Cool allows users to automatically adjust the direction of air flow based on the temperature at the air outlet. Hence, you can set the temperature a few degrees higher as well while keeping the conditions within the space as comfortable as before. Additionally, this feature also increases energy efficiency by about 20%.
- 7-way airflow for better efficiency – A unique feature brought about by Mitsubishi Electric, this allows users to adjust the flow of air to 7 directions horizontally and 6 directions vertically. Ensuring the flow of air to 42 different directions, this step offers the benefit of maximum control over air directions. Thanks to this, air conditioning can be utilized in areas where it is actually required.
- Computerized dehumidification – Another exceptional function in the MS-GK series of air conditioners by MEI, computerized dehumidification enables you to avoid dampness within your living space, without having to lower temperatures. You can, therefore, enjoy more comfortable and healthier air conditioning, alongside the all-year round economy.
Other factors that make it a great choice
- Nano Platinum Filter - The filter within the MS-GK series air conditioners comes with nanometre-sized platinum ceramic particles that destroy bacteria along with deodorizing the circulating air. This filter also ensures better dust collection in comparison to ordinary ACs.
- Wide & Long Airflow – These air conditioners come with a remote control that allows you to automatically control the left vane for better comfort. Again, by using the wide vane mode, you can adjust the direction of airflow to reach any corner within a given space. The high-power motor coupled with a newly designed long mode pushes the air further out to offer extended air flow that can reach far ends of the room.
- LCD Remote Control – With the MS-GK series of air conditioners, you get to customize your environment, be it in terms of temperature, air volume, operation or direction, simply by the touch of a button. The large buttons make it easy to use frequently-used functions, and the LCD display lets you keep a tab of temperature and other operating conditions.
- Electrostatic Enzyme Filter (Optional) – Charged with static electricity, the filter fitted in the MS-GK series air conditioners trap and decompose allergy-causing elements like bacteria and moulds by the use of enzymes retained in the filter.
As a buyer, it is time to be prudent. Look for more than just cooling in an air conditioner that you buy. Buying an air conditioner like Mitsubishi Electric’s MS-GK series of ACs will help ensure that Nature does not have to pay for the comfort you gain.
09 JULY 2019