IT COOLING SYSTEMS
1 Nov. 2022
Iran Khodro IKCO, founded in 1962, is an Iranian multinational automaker with headquarters in Tehran. IKCO manufactures vehicles under different brands including Samand, Peugeot, and Renault in 12 production sites around the word. Expanding its markets to Central Asian countries including Kirgizstan and Azerbaijan as well as Central and North African countries are the main goals of this car company.

With such challenging development prospects for the next several years, it is easy to understand why the company decided to create its own data center, at its headquarters.

To cool the whole IT facility while guaranteeing a high efficiency of the structure, the M&E designers have selected 11 ACU close control units and 5 big chillers, all Climaveneta branded. Specifically 2 FOCS/B 1942, 2 FOCS/K 1702 and 1 NX/CA 0714T have been selected to cool the data center, while 2 further NX small chillers have been installed to grant the perfect internal comfort for the administration offices.