Reducing carbon emissions, electricity consumption, and minimizing stress on the environment are what encompass the concept of sustainability. The aim is to focus on technological progress while conserving the resources that this world provides us. In that regard, it has become important for global brands to take the lead on this front, and that is exactly what Mitsubishi Electric does - we make sustainable electric solutions keeping in mind the balance of the world’s delicate ecosystem.
Being a strong advocate of sustainability, Mitsubishi Electric takes care of several aspects that surround its electric solutions. Take a look at our portfolio that underlines our focus on sustainability: -
Mitsubishi Electric air conditioners are developed with the utmost care for the environment in mind. The MSY GR(T) Series, for instance, employs the Inverter Power Module that adjusts the frequency in a way that it reduces the overall power consumption. In addition to that, the motor in the compressor uses dense winding technology for enhanced efficiency.
Mitsubishi Electric’s drive products within the Factory Automation category do their own bit for sustainability. For instance, the range of Inverters – FREQROL has regenerative braking torque for higher energy efficiency and to ensure less wear and tear. Additionally, these inverters have an overall energy-efficient design.
In a bid to enhance building systems, Mitsubishi Electric offers a range of elevators with a strong focus on sustainability.
Mitsubishi Electric is the first company in the world to use a high capacity All-SiC (Silicon Carbide) power module in the inverters employed in rail car systems. The All-SiC power module fitted traction inverter offers 40% energy savings in terms of power consumption!
That is not all; the All-SiC power modules in these inverters provide an energy-efficient design for the rail car systems and contribute to a transportation system with a significantly reduced carbon footprint.
With the help of the Full SiC DIPIPM, air-conditioners have become more power efficient than ever. Because the SiC (Silicon Carbide) MOSFET decreases the ON resistance, the power loss decreases by 70% (approx.) in comparison to conventional air conditioners. With such a huge percentage of reduction in power loss, the Full SiC DIPIPM by Mitsubishi Electric contributes to a more sustainable environment.
Furthermore, thanks to the material characteristics of SiC, power electronic devices help in substantial energy savings while also reducing the overall carbon footprint.
The world today calls for sustainability. Whether it is about how we use resources or how we preserve them, the one fact that is undeniable is that we have to be judicious in our ways. As a brand, Mitsubishi Electric doesn’t just promote the cause of sustainability; it advocates this belief through its range of sustainable and energy-efficient product range. After all, it is important to put a sustained effort to achieve a better tomorrow.