Dirt and dust are some of the biggest enemies of air conditioners. They slow down the machines and fail to cool the room. Once the damage is too heavy, there may even be a need for replacement or the concurrent repair costs may prove to be cumbersome.
Air Conditioning area generally contains different types of dirt. Classified into two groups, hydrophilic dirt refers to dirt such as fiber dust and sand dust and hydrophobic dirt is dirt such as oil and cigarette smoke.

At times when the inside components of Indoor Air conditioners are left dirty, the consequences can be harmful to the unit. There are chances that the Air Flow volume is reduced, the Air Conditioner may get moldy, the outlet air may smell bad or there may be deterioration in the energy efficiency of the Air conditioner system.
An advanced technology that protects air conditioners from the ill effects of dirt and dust is the dual barrier coating technology. This technology helps in reducing the attachment of dust and oil mist that coats the inside of the conditioners. The coating material greatly reduces the attachment of dust which is mixed in the air. This lends the units the power to work at full performance. The reduction in dirt also means the bad smell and odours godown. With less dirt, the necessity of cleaning the air conditioner also lessens.
Another upside of the dual barrier coating technology is its green effects. The technology is environment friendly and does not cause harm to the ozone. Currently, the air conditioners from Mitsubishi Electric use the dual barrier technology in its unit. Mitsubishi Electric offers “Dual Barrier Coating” which works as a two barrier coating with blended fluorine particles that prevent hydrophilic dirt penetration and hydrophilic particles that prevent hydrophobic dirt from getting into air conditioner. This dual coating on the inner surface keeps the air conditioner clean round year.

Mitsubishi Electric’s units are equipped with a sophisticated, streamlined design and a comprehensive range of features to make stylish, energy efficient air conditioning available for countless small businesses. These also consist of Double vanes on the indoor unit that operate independently to distribute airflow evenly throughout the room and the company’s MSZ-LN offers a whisper-quiet operation as low as 19 dB(A). A Plasma Quad Plus filter also uses powerful plasma technology to filter out even microscopic particles, whilst the dual-barrier coating on the heat exchanger, fan and air duct prevents dust and grease accumulation. The company offers Dual Barrier Coating in their current model MSY-GN & MSZ-LN and in the upcoming model MSY-JP.
The cutting-edge technology is one of the latest additions to the company’s repertoire of advanced technologies.